{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the dimensions of the door handle cutout on the NetShelter SX?
Issue:
We are being asked to provide the dimensions of the door handle cutout.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers wishing to use a 3rd party door handle need to know the size of the door handle cutout.

Resolution:
The dimensions of the NetShelter SX door handle cutout are: (H) 150 mm x (W) 25.5 mm.  (6" x 1")

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: