{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

What is the 2nd motor parameters in ATS48?


The 2nd set of parameters are used when we have two different motors are to be operated separately where we can save the parameters of each motor separately & switch between the two configurations using a logic input ( the logic input in the I/O menu is to be set to LIS, so for example LI3 or LI4= LIS ) so they can be started one after the other using a single soft starter
Noting that switching from one parameter set to another can be done if ATS is not driving the motor (ATS in stop state). Below attached those parameters
Explore more
Explore more

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.