{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Safety limit switches XCS - How to order the XCSZC590L01M8 part number ?

Find attached the picture of both part XCSZC1 magnet and XCSZC590L01M8 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMC590L01M8. This is the commercial reference to order to get the XCSZC590L01M8 switch with the magnet XCSZC1, sold into the same packaging plastic bag. The following rule can be applied to all XCSDMC magnetic switches : XCSZC1 + XCSZC59* (or XCSZC79*) = XCSDMC59* (or XCSDMC79*) complete magnetic switch; e.g. XCSZC1 + XCSZC5912 = XCSDMC5912 commercial ref

Schneider Electric Nigeria

Attachment(s)

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.