{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does the NetShelter WX castor kit AR8359 fit onto the AR106, AR109 or AR112.
Issue:
There doesn't appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
There is a request to add castors to AR106, AR109, AR112, AR106SH4, AR109SH4, AR112SH4, AR106SH6, AR109SH6, AR112SH6, AR106V or AR106VI.

Resolution:
There is no castor kit for the AR106, AR109 or AR112.
The smallest cabinet that has a castor kit available is the AR100  and AR100HD. They use AR8359 available as a castor kit.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: