{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Does the Magelis / Harmony series of HMI offer remote access to see the screen via a local or wide area network?

Issue:
Does the Magelis / Harmony series of HMI offer remote access to see the screen via a local or wide area network?

Product Line:
HMIGTO/GTU/STO/STU, XBTG/GC/GH/GK/GT, iPC, Compact, Smart, Flex Box, Box PC, Panel PC

Resolution:
With the current version of Vijeo Designer, v6.2, there are two options to remotely access the Magelis / Harmony targets.  One option is Web Gate using Internet Explorer with Windows operating systems.  The other is to purchase and use an iOS or Android app called Vijeo Design'Air.

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.