{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What's the difference between the new SP shock packaging and the previous SP1 and SP2 products?
Issue:
An explanation is needed to distinguish between the SP1 and SP2 versions and the new SP shock packaging.

Product Line:
NetShelter SX Shock Package

Environment:
All versions and serial ranges.

Cause:
All of the SP1 and SP2 shock packaging skus have been replaced by AR3xxxSP skus.

Resolution:
For a complete list of the differences in the new and old shock packaging please see the attached document.

Here are a few of the basic differences:

Pallet - more robust and size.
Ramp - more robust, single piece vs multiple pieces.
Protection - foam vs cardboard corner protectors.
Cabinet - additional mounting rail fasteners secure the mounting rails to the side brace.
-Cabinet elevation brackets (4) installed at the bottom of the cabinet and allow the cabinet to rest on the pallet bracket versus the casters during shipment.
-Casters - heavy duty and fixed rear castors.
Pallet bracket - easy removal methods (2 possible methods) , includes feet for the cabinet to rest on and elevate the cabinet removing the weight of the cabinet and its contents from the casters during shipment
More sizes available - now different heights and depths than the standard

Schneider Electric Nigeria

Attachment(s)
Shock_Packaging_Overview_Presentation.pdf [756.31 KB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: