Issue:
This document contains a video on how to change the temperature thresholds on a Network Air FM unit.
Product line:
FM35-50, ACFM, IR40.
Environment:
All Serial Numbers.
Cause:
Install Operation.
Resolution:
How to change the temperature thresholds on a Network Air FM unit follow the below procedures.
1 Press ESC until you reach the main menu (On/Off).
2 Scroll to SETUP and press ENTER.
3 Scroll to SYSTEM 1 and press ENTER.
4 Press ENTER on ALARMS.
5 Press ENTER on TEMPERATURE THRSHLD.
6 Select which threshold you want to change and then press ENTER.
7 Use the UP or DOWN arrows to select the desired temperature.
8 Press ENTER when finished.
9 Press ESC until you get back to the status screen.
This document contains a video on how to change the temperature thresholds on a Network Air FM unit.
Product line:
FM35-50, ACFM, IR40.
Environment:
All Serial Numbers.
Cause:
Install Operation.
Resolution:
How to change the temperature thresholds on a Network Air FM unit follow the below procedures.
1 Press ESC until you reach the main menu (On/Off).
2 Scroll to SETUP and press ENTER.
3 Scroll to SYSTEM 1 and press ENTER.
4 Press ENTER on ALARMS.
5 Press ENTER on TEMPERATURE THRSHLD.
6 Select which threshold you want to change and then press ENTER.
7 Use the UP or DOWN arrows to select the desired temperature.
8 Press ENTER when finished.
9 Press ESC until you get back to the status screen.
Released for:Schneider Electric Nigeria