{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Do the CSH120 and CSH200 CTs work with VAMP relays?
Product Line
VAMP

Resolution
Yes, the CSH120 and CSH200 core balance CTs will work on the VAMP relays so long as the CT inputs are the 1A / 0.2A input option.

Note:  See attachment for instructions on using the CSH CT's with the VAMP relays.

Schneider Electric Nigeria

Attachment(s)
Using-CSH120-with-VAMP-protection-relay-range.pdf [115.55 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.