{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Safety light curtains XU - Housing cross-section of the XUSL4MA or XUSL4MB safety light curtains

Housing cross-section of the XUSL4MA or XUSL4MB safety light curtains with built-in muting function = 50mm x 55mm. See attachment

Attachment(s)

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.