undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Nutanix Files does not shut down when vCenter Server is deployed as a VM on Nutanix Cluster
Issue:
Nutanix Files does not shut down when vCenter Server is deployed as a VM on the Nutanix Cluster.

Product Line:
PowerChute Network Shutdown v4.3

Environment:
PowerChute configured with Nutanix support with VMware as hypervisor; vCenter Server deployed as a VM on the Nutanix Cluster; Nutanix Files 3.0, 3.1, 3.2

Cause:
Nutanix Files VMs do not have VMware Guest Tools installed, which prevents PowerChute from retrieving their IP addresses in order to stop Nutanix Files Cluster via SSH. This issue only occurs where vCenter Server is deployed as a VM on the Nutanix Cluster.

Solution:
Update Nutanix Files to version 3.5

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: