undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Will a short-depth Smart-UPS fit into the NetShelter WX AR106 or AR109 wall box?
Issue:
Need to check mounting depth of the UPS, and available space between the front mounting rails and rear of the wall box.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
The new Short Depth UPS may fit into a small wall box.

Resolution:

The new Short Depth Smart-UPS will not fit into AR106 or AR109 because there is not enough room to connect power cords into the UPS.
The AR106 and AR109 have about 13" of available mounting depth, as measured from the front mounting rails to the rear of the cabinet.
A UPS would need to have a mounting depth of 11.25" or less to allow room power cords to plug in.

You can also find compatibility to all NetShelter cabinets and APC products by Googling "netshelter accessory compatibility chart" and pulling up FAQ 158651: https://www.apc.com/us/en/faqs/FA158651/

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: