{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the distance between PDU mounting holes on the NetShelter SX accessory rails?
Issue:


Product Line:


Environment:
All versions and serial ranges.

Cause:


Resolution:

In the 42U cabinet
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25")

In the 45U cabinet
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25")

In the 48U cabinet
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25")

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: