{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are the 8911DPS starters provided with a NO holding contact?

Issue:
Do the 8911DPS starters come with a normally open holding circuit?

Product line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8911 Type DPS NEMA Definite Purpose Starters

Cause:
Customer control wiring

Resolution:
No, the Class 8911DPS starters do not come with any auxiliary contacts as standard.  These can be ordered with auxiliary contacts from the factory, or some can be field installed.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.