{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to work with the Control Expert spanned files that you downloaded.
Issue
Working with 7-zip spanned files

Product line
Control Expert

Resolution
1. Must have or need to Install 7zip (www.7-zip.org).
2. Right Click on the xxxxZ.001 file and select 7-Zip -> Extract.
3. This creates a single ISO file. If you are familiar with ISO files then use is as you like, otherwise go to step 4.
4. Right Click on the ISO file and select 7-ZIP -> Open Archive to see all of the folders, then extract them to a location on your hard drive.
5. Launch Setup.exe to install Control Expert.

Schneider Electric Nigeria