undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What size panel (or range) does the NetShelter cage nut fit?
Issue:
The panel range for NetShelter cage nuts is requested.

Product Line:
NetShelter SX, SV, VX and WX hardware.

Environment:
AR8100, AR8005

Cause:
Extra cage nuts are needed and must be sourced locally.

Resolution:

The NetShelter cage nut panel range is 1.6mm - 2.0mm. This equated to a 14 awg to 16 awg panel.
All cage nuts provided by APC for NetShelter cabinets use this size, regardless of nut/screw combination.

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: