Browse FAQs

What is the maximum number of devices can be added to MPM?

Published date: 12 March 2021

A Device in the context of Building Expert is a hardware specifically designed to provide monitoring, power consumption, or room comfort control.
Devices can be one of the following:
  • Power Meter
  • Room Controller
  • Sensors
  • Relays
Devices are added directly from Building Expert. The Add Device icon on the toolbar opens a new window allowing you to add any Device to your project.
You can only add a maximum of 49 Devices to each MPM. This limitation applies to adding either 49 of the same Device type, or, a combination of several Device types.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.