undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
PowerChute Network Shutdown fails to shut down all hosts in a vSAN Cluster when using Advanced UPS Configuration with FTT Support enabled.
Issue:
PowerChute Network Shutdown does not complete the shutdown sequence for the vSAN hosts when UPS critical events occur on multiple different UPS setups at the same time in an Advanced UPS configuration with FTT support enabled.

Product:
PowerChute Network Shutdown version 4.3

Environment:
PowerChute Network Shutdown installed on Windows OS, configured for Advanced UPS configuration with FTT enabled.
Cause:
Software issue.


Solution:
1. Download the attached pcns_vsan_ftt.zip file.
2. Uncompress the file.
3. Open command prompt as an administrator and stop the PowerChute service net stop pcns1
4. Rename C:\Program Files\APC\PowerChute\group1\comp\pcns.jar to original_pcns.jar
5. Copy the uncompress pcns_vsan_fft.jar file to C:\Program Files\APC\PowerChute\group1\comp and rename it to pcns.jar
6. Start the PowerChute service net start pcns1

Schneider Electric Nigeria

Attachment(s)
pcns_vsan_ftt.zip [2.38 MB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: