Browse FAQs

Can you freeze the DM6000 meter screen on a specific parameter, instead of circulating parameters?

Published date: 19 January 2021

Issue:
Can you freeze the DM6000 meter screen on a specific parameter, instead of circulating parameters?

Environment:
PowerLogic DM6000 series

Resolution:
The meter screen can be locked at your preferred parameters.

This can be done through holding the up and down buttons simultaneously for 2 seconds at the preferred screen.

This will lock the meter display to this screen. However, the screen will change if someone navigated to other screens.

If you went to other pages afterwards, the meter will go back to the previously locked screen after 4 minutes.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.