{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the password used for the Zelio relay inside the enclosed ATV660 Drives?

Issue:

ATV660 enclosed Zelio relay password

Product Line:

ATV660, ATV960

Environment:

All

Cause:

Needs to access the password to look at the program or to change the program.

Resolution:

The default password for the Zelio relay is 6601 however according to the manufacturing plant some may have been shipped out with password 6101 and 6201.

Schneider Electric Nigeria

What is the password used for the Zelio relay inside the enclosed ATV660 Drives?

Issue:

ATV660 enclosed Zelio relay password

 

Product Line:

ATV660, ATV960

 

Environment:

All

 

Cause:

Needs to access the password to look at the program or to change the program.

 

Resolution:

The default password for the Zelio relay is 6601 however according to the manufacturing plant some may have been shipped out with password 6101 and 6201.

Schneider Electric Nigeria
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
move-arrow-top