{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How to to unlock the drive using master reset password for ATV310 ?

1. Go to the 999. Press Enter. ON will be displayed ( meaning drive is password protected and hence access to FULL menu and factory reset is not permissible) 2. Rotate jog dial clockwise and set...

What is the function of the Unika Sockets with interlock switch ?

In conformity with IEC 60309 standards, all the industrial sockets have a lock or holding mechanism, which keeps the plug firmly locked in the socket, preventing it from being pulled out...

What is replacement of eocrss-30s ?

kindly be informed that EOCR is under Samwha which is not locally offered and this range in commercilaized only in South Korea. However, kindly find attached the commercialized in Schneider product...

ATV61EX**** drive trips with "Internal thermal sensor fault - THSC" as...

The fault happens due to the defective temperature sensor - installed in heat sink of the drive. The temperature sensor can be defective either by short circuit or open circuit. The fault message...

What are the different license sizes of Unity Pro 11 ?

Unity Pro V11 is available in 3 different sizes : S, L, XL The only difference between sizes S, L, XL is the supported controller references. Supported PLCs by size :

What is the difference between isolation and disconnection for any switch...

Isolation : it is switching the ciruit to open it with a suitable space between moving and fixed contact to prevent ionization of air in this space ( complete safety ) Disconnection : it is switching...

Can i use Vigirex residual current relays for 3-wires systems with no...

The Vigirex residual current relays, combined with a toroid, provide protection against earth leakage currents for all LV electrical network types less than 1000 V, regardless of the type of earthing...

What is the thickness of the Steel sheet metal used in Okken switchboard.

The Steel sheet metal thickness used in Okken switchboard is as listed below: Okken Steel sheet metal thickness Housing Thickness mm Door 2.00mm Rear panels 1.50mm Side panels 1.50mm Roof 1.50mm...

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our Generic Knowledge FAQsGeneral Knowledge

What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...