what is replacement for LC1D8011M7 ?
LC1D8011M7 is replaced by LC1D80M7
{}
LC1D8011M7 is replaced by LC1D80M7
1-For Compact NSX: the required trip unit with adjustable Long time protection (L)and short time protection(S) with instantaneous protection (I) can be achieved with Micrologic 2 trip unit taking...
1. Go to the 999. Press Enter. ON will be displayed ( meaning drive is password protected and hence access to FULL menu and factory reset is not permissible) 2. Rotate jog dial clockwise and set...
Generally the motor with Class F insulation is considered as VFD graded motor, but it is specified that the dV/dT withstand capacity is 1 KV/μS. Hence we can not consider this motor as VFD graded...
issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...