Does Compact NS/NSX Switch Disconnector (NA) have the Reflex Tripping feature.
Yes, Reflex Tripping is available in all Compact NS/NSX Switch Disconnectors.
The threshold of the Reflex Tripping auto-protection is about 20 x In and time delay is less than 10 ms.
The Reflex Tripping is due to "Piston - which is purely mechanical" and not due to the trip unit.
Thus the Reflex Tripping being a mechanical controlled function is also available in the Compact NS/NSX Switch Disconnectors.
According to IEC947 directive Switch Disconnectors with this protection functionality may NOT be used as protection devices as stand alone solution.
The threshold of the Reflex Tripping auto-protection is about 20 x In and time delay is less than 10 ms.
The Reflex Tripping is due to "Piston - which is purely mechanical" and not due to the trip unit.
Thus the Reflex Tripping being a mechanical controlled function is also available in the Compact NS/NSX Switch Disconnectors.
According to IEC947 directive Switch Disconnectors with this protection functionality may NOT be used as protection devices as stand alone solution.