{}

Veelgestelde vragen (FAQ's) zoeken

{"searchBar":{"inputPlaceholder":"Op trefwoord zoeken of een vraag stellen","searchBtn":"Zoeken","error":"Voer een trefwoord in om te zoeken"}}

Is it possible to use circuit breaker iC60 for operatingvoltage 480VAC?

Article availabe in these languages: Engels, Nederlands

The circuit breaker iC60 is for a maximal operatingvoltage 440VAC.
There is a voltagetolerance of 10% but it is dedicated only for voltagefluctuation of distribution network.
The iC60 should not be used in distribution network with nominal voltage of 480VAC.

We recommend to make use the NG125-series instead, which has operatingvoltage up to 500VAC.

Bent u geholpen met deze informatie ?

Ontdek meer
Productfamilie
Acti9 iC60Acti9 NG125
Ontdek meer
Productfamilie
Acti9 iC60Acti9 NG125