{"searchBar":{"inputPlaceholder":"Op trefwoord zoeken of een vraag stellen","searchBtn":"Zoeken","error":"Voer een trefwoord in om te zoeken"}}
{}

Welkom op de website van Schneider Electric

Welkom op onze website.

Kies uw locatie

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Ja","noButton":"Nee","feedback":{"title":"Wat kunnen we doen om dit te verbeteren?"},"submitButton":"Verzenden","successMessage":"Bedankt voor uw feedback","title":"Bent u geholpen met deze informatie ?","feedbackPercentLabel":"van de mensen vonden dit nuttig","captcha":{"error":"Vink het vakje aan"}}}
Veelgestelde vragen (FAQ's) zoeken

Allowed operating temperature for limiter LA9LB920

Ambient operating temperature for the limiter LA9LB920 is not a subject in catalogue or datasheet, because the LA9LB920
is not a stand-alone product but just accessory for TeSys GV2 or U.
Therefore the ambient air temperature for operating is equal to the products which it is used with (TeSys GV2 or U).
The Ambient air temperature for operating of TeSys GV2 or U is specified in TeSys catalogue and customer can use the same values for LA9LB920.
For example, if LA9LB920 is used in combination with GV2ME,  then ambient air operating  temperature is: -20…+60°C ( open air mounted )  or -20…+40°C mounted in enclosure.
 
Ontdek meer
Productfamilie
TeSys D

Vindt u niet wat u zoekt?

Neem contact op met ons Customer Care-team voor technische ondersteuning, hulp bij klachten en meer.
Ontdek meer
Productfamilie
TeSys D