{}

Søk i ofte stilte spørsmål (FAQ)

{"searchBar":{"inputPlaceholder":"Søk etter nøkkelord, eller still et spørsmål","searchBtn":"Søk","error":"Skriv inn et søkeord"}}

What are the Auxiliaries that can be used with C60H-DC.

Article available in these languages: Finsk

Refer the attached documents for the list of Auxiliaries that can be used with C60H-DC.

1. For the list of Auxiliaries that can be used with C60H-DC as per IEC certification refer attachment 90081.pdf
2. For the list of Auxiliaries that can be used with C60H-DC as per UL certification refer attachment 91103.pdf

Vedlegg

90081.pdf90081.pdf [924.75 KB]
91103.pdf91103.pdf [788.71 KB]

Var dette nyttig?

Finn ut mer
Rekkevidde:
C60 for DC
Finn ut mer
Rekkevidde:
C60 for DC