{"searchBar":{"inputPlaceholder":"Søk etter nøkkelord, eller still et spørsmål","searchBtn":"Søk","error":"Skriv inn et søkeord"}}
{}

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.

Velg din lokasjon

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Ja","noButton":"Nei","feedback":{"title":"Hva kan vi gjøre for å bli bedre?"},"submitButton":"Send inn","successMessage":"Takk for din tilbakemelding","title":"Var dette nyttig?","feedbackPercentLabel":"av personer syntes dette var nyttig","captcha":{"error":"Huk av i boksen"}}}
Søk i ofte stilte spørsmål (FAQ)

What is the difference between tLIN and tLIG parameter setting in Altivar 32 drive.

tLIM permit to limit the torque when the motor is in motoring mode and tLIG permit to limit the torque when the motor is in generator mode.
So, these functions permit to limit the motor available torque,for example in case of motor mode, if torque need by application increased more
than the limit ,then the speed will decrease and the torque does not exceed the limit,and not to stop the motor when the limit is reached.

Note:
tLIM means Motoring torque limit
tLIG means Generator torque limit
Finn ut mer
Rekkevidde:
Altivar 32
Finn ut mer
Rekkevidde:
Altivar 32