{"searchBar":{"inputPlaceholder":"Søk etter nøkkelord, eller still et spørsmål","searchBtn":"Søk","error":"Skriv inn et søkeord"}}
{}

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.

Velg din lokasjon

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Ja","noButton":"Nei","feedback":{"title":"Hva kan vi gjøre for å bli bedre?"},"submitButton":"Send inn","successMessage":"Takk for din tilbakemelding","title":"Var dette nyttig?","feedbackPercentLabel":"av personer syntes dette var nyttig","captcha":{"error":"Huk av i boksen"}}}
Søk i ofte stilte spørsmål (FAQ)

Is there a bit in the TWDLCAA40DRF and TWDLCAE40DRF Twido controllers, that gives the status of the external battery?

Issue: 
System status bit for the external battery


Product Line:
Twido PLC


Resolution:
Yes it is System bit %S75.
This system bit is set by the system.
It indicates the external battery status and is readable by the user:

text Set to 0, external battery is operating normally,
text Set to 1, external battery power is low, or external battery is absent from compartment.