Søk i ofte stilte spørsmål (FAQ)
What are the differences between the AS-P810-000 and the AS-P810-001 power supplies?
Issue
Suitable replacement for the P810 power supply.
Product line
984 800 series
Environment
P810 power supply
Resolution
Both models of the P810 operate from either a 115VAC or 230VAC power line. The P810-001 includes a power on/off keyswitch and a front accessible fuse. The P810-000 does not offer these two features. With the exception of the keyswitch and the front-mounted fuse, the two power supplies are identical.