{}

Søk i ofte stilte spørsmål (FAQ)

{"searchBar":{"inputPlaceholder":"Søk etter nøkkelord, eller still et spørsmål","searchBtn":"Søk","error":"Skriv inn et søkeord"}}

What is the maximum number of Control Expert DTM implicit connections supported on the BMXNOC0402 module?

Issue
Need to specify the maximum number of connections supported on BMXNOC0402 module configured through the Control Expert DTM browser.

Product Line
Modicon M580
BMXNOC0402

Environment
ODVA Ethernet/IP
Control Expert DTM Browser

Resolution
The BMXNOC0402 supports a maximum of 128 device connections configured through the Control Expert DTM Browser capability.

Var dette nyttig?

Finn ut mer
Rekkevidde:
Modicon M340
Finn ut mer
Rekkevidde:
Modicon M340