{"searchBar":{"inputPlaceholder":"Søk etter nøkkelord, eller still et spørsmål","searchBtn":"Søk","error":"Skriv inn et søkeord"}}
{}

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.

Velg din lokasjon

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Ja","noButton":"Nei","feedback":{"title":"Hva kan vi gjøre for å bli bedre?"},"submitButton":"Send inn","successMessage":"Takk for din tilbakemelding","title":"Var dette nyttig?","feedbackPercentLabel":"av personer syntes dette var nyttig","captcha":{"error":"Huk av i boksen"}}}
Søk i ofte stilte spørsmål (FAQ)

How does smart mode reporting work in PME 7.2.3 and PME 8.x?

Issue:
Smart mode reporting was a feature introduced in Power Monitoring Expert 7.2.3 for select reports. There is a need for a technical document which explains which reports support this feature, as well as which measurements are part of this feature.

Product Line:
Power Monitoring Expert 7.2.3
Power Monitoring Expert 8.x

Environment:
Power Monitoring Expert Software Configuration

Cause:
There are limitations to smart mode reporting in Power Monitoring Expert 7.2.3. It will only work with the select reports templates (Tabular, Trend, Multi Device Usage, Single Device Usage, and Hourly Usage Report).
Additionally, it will only work with Hierarchy nodes and only supports a limited set of measurements. Documentation is needed to understand it's limitations.

Resolution:

The attached document is a technical reference which explains the limitations and use case for smart mode reporting.
 
Finn