{}

Søk i ofte stilte spørsmål (FAQ)

{"searchBar":{"inputPlaceholder":"Søk etter nøkkelord, eller still et spørsmål","searchBtn":"Søk","error":"Skriv inn et søkeord"}}

Osisense XC - Do we have a ZCE02 head suitable for marine environment

We can propose the adapted ZCE02N head designed for such environment (N=Navy), designed to be mounted on a plastic body in XCKN series (adapted switches) or in standard XCKP model. All the steel parts are in stainless steel : roller, roller axis, internal spring, plunger roller. The plunger holder has a special plating for this environment. Such special head is available to order in December 2020 (logistic reference ZCE02NA)

Var dette nyttig?

Finn ut mer
Finn ut mer