Issue
The Schneider Electric CoreServiceHost service needs to connect to PowerSCADA Runtime through a valid Username/Password (defined in PowerSCADA project) and Citect I/O Server IP Address.
Product Line
PowerSCADA Expert 8.1
Environment
Windows Services
Application Configuration Utility
Cause
A change in server IP address or removing the 'user' defined in PowerSCADA Project. The status of the Schneider Electric CoreServiceHost service will continue to show as 'running', however, it is not connecting to PowerSCADA Runtime.
Resolution
Open a browser and type the following for the URL: http://localhost:23103/CoreServiceHost/Alarms/AlarmProxy/status
When a connection can be made, the following message is returned:
When a connection cannot be made, the following message is returned:
Note: In the latter case, the problem can further be investigated in Application Configuration Utility by checking the Username/Password and server IP Address.
Publisert for: Schneider Electric Norway