Hvordan kan vi hjelpe deg i dag?

What's the difference between the BR20 and BR21 Base Radios?

The accutech BR20 Base Radio only supports modbus RTU protocol using serial RS232 or RS485 communications and the accutech BR21 Base Radio only supports modbus/TCP protocol.