{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

What is the ATV58 Power loss ride through time?

Issue:
ATV58 Power loss ride through time

Product Line:
 ATV58

Environment:
 Power Loss ride through

Cause:
 n/a

Resolution:
Ride through depends upon the inertia of the load, control wiring, power wiring and drive settings.

When IPL (Input Phase Loss) is disabled and StP (Controlled Stop) is set to MMS, the DC Bus is kept energized by the kinetic energy from load inertia until USF(Undervoltage fault occurs).

Additionally, if Atr (autorestart) is set to YES, two-wire control (tCt) with level detection (LEL) is set and power is lost to the drive for longer time periods and then restored, the drive will restart if the run command is present.

Typically, the limiting factors for ride through are electromechanical relays and contactors rather than the drives. The DC bus capacitors used in AC drives allow the control voltage to remain present much longer than loss of AC line voltage. Relays and contactors tend to open quickly on loss of power.

 
Explore more