{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Is it possible to find out the project name that is in the Magelis HMI runtime?

Issue:
Is it possible to find out the project name that is in the Magelis HMI runtime?

Product Line:


Environment:


Cause:


Resolution:
It is not possible to determine the project name of the Magelis in runtime.  But there are two possible work around to display the project name.  You can use a script ,Sys.getInfoString(PROJECT_NAME), to retrieve the project name write it to a string variable.  Or from Web Gate, under Project link of the diagnostics tab, it will display the project name.
Explore more
Explore more