{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Will TSXSAY100 communicate with a TeSys LF3MP06EU ?

Issue: Compatibility


Product Line: TSX Platform,


Environment: ASi


Cause: version difference


Resolution:

In our Catalog, we have two Asi Primaries:

TSXSAY100    ASi V1
TSXSAY1000  ASi V2.

The TesysLF range use ASi V2 component. They use extended addressing. (i.e., use two banks of addresses).

Hence  a Primary ASi V2 is mandatory and hence the TSXSAY100 must be replaced by TSXSAY1000.

Detailed information:

If we manage a secondary ASi V2 with a primary ASi V1 there are some restrictions as listed below:
Only a maximum of 31 secondaries is supported.
V2 secondaries have the option to address 1-62 instead of 1-31 (or to be more
exactly 1a-31a and 1b-31b), while a V1 device will use both addresses
(a+b) as they "don't know about the 'b' side."

In case of a periphery fault :
The secondaries are not inhibited ( in our offer )
the primary can ’t manage the periphery fault information from the secondary

=> The PLC can ’t differentiate an open contact and an input supply short-circuit.
=> The operator is not warned of output short-
 
Typically a primary V1 cannot handle extended addressing.
From a V2 secondary device point of view, typically the profile(s) are not supported by the V1 primary.

Hence the recommendation to use a TSXSAY1000 which is a ASi v2 primary, with a TeSys LF3MP06EU