{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is part number for 4 pole, 80A contactor , 220V DC Coil?

The part number for 4 pole, 80 A contactor , 220V DC Coil is LP1D80008MD. This Contactor is AC-1 rated only (Slightly Inductive Loads/resistive loads).
https://www.se.com/au/en/product/LP1D80008MD/tesys-d-contactor---4p%282-no-%2B-2-nc%29---ac-1---%3C%3D-440-v-125-a---220-v-dc-coil/

For more details refer the following link to the catalogue.
https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=MKTED210011EN.pdf&p_Doc_Ref=MKTED210011EN

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.