{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

What standards do EM4200 Enercept meters comply with?

Product Line
EM42xx Enercept meters
EM4235
EM4236

Environment
Declaration of standards compliance

Resolution
The EM42xx Enercept meters comply with the following
Safety:EN 61010-1:2010  
 UL 61010-1:2012
 
  
EMC:EN 61000-6-2:2005 Immunity 
 EN 61326-1:2013  
    
 EN 61000-6-3:2007+A1:2011EmissionsClass A
 EN 61326-1:2013  
    
 EN 61000-3-2:2014Harmonics 
    
 EN 61000-3-3:2013Flicker 
    

EM42xx Enercept meters also comply with the requirements of the following
  1. The Low Voltage Directive 2014/35/EU
  2. The EMC Directive 2014/30/EU
  3. The RoHS Directive 2011/65/EU
and bear the "CE" mark accordingly. 

A signed copy of the Declaration of conformity for EM42xx Enercept meters can be downloaded below