Browse FAQs

Why is LED Light not working correctly with 750WP?

Published date: 17 December 2019

Unfortunately LED Lights are not a compatible load type of the 750WP.
If you are controlling a LED load and a sensor is required, you will need to use a 3-Wire version. The part number for a 3 Wire version is a 750WPR.
Please see the compatibility chart below:
Catalogue Number 750WP 750WPR
Compatible Load Types Incandescent Incandescent
  240V Halogen 240V Halogen
  Iron Core Transformers Fluorescent Loads
  N/A Iron Core Transformers
  N/A Electronic Transformers
  N/A Shaded Pole Induction Motors (Exhaust fans, (5A Max)
  N/A Split Phase Induction Motors (ceiling fans, 5A Max)
  N/A Other Motor Loads (Limit to 5A Max)
Incompatible Load Types Electronic Transformers N/A
  Fluorescent Loads N/A
  Discharge Lamps N/A
  Motor Loads N/A

Some of the key features for the 3 wire 750WPR Outdoor sensor are:
  • 10A maximum load current
  • Stand-by power consumption is less than 1W
  • 3 Wire
  • Neutral required
  • 30 seconds warmup time
  • 18 metre radius x 110° rated detection field at maximum sensitivity
  • 5 seconds to 20 minutes timer delay range
  • Cables accommodates 4 terminals, up to 2 x 2.5mm² cable per terminal
  • Relay switching method
For further information please visit https://www.clipsal.com/products/detail?CatNo=750WPR&tab-document-1=0



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.