{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

E-Flex HOA is acting in reverse the Hand is looking at the 4 to 20mA signal and the Auto is looking at the HMI for speed control.

Issue:
E-Flex HOA troubleshooting

Product Line:
E-Flex

Environment:
All 

Cause:
Programming is backwards for Ref 1 and Ref 1b.

Resolution:
Set up your Access level to advanced
Menu 1.2 check the status of your logic inputs LI3 your HOA logic input. 
Hand=1
Off=0
Auto=0

Basic programming to match up HOA inputs
REf 1 channel set to AI2
REf 1b channel set to HMI
Profile is SEP
Command switching is channel 1 active
CMD channel 1 is Terminal. 

 
Explore more
Explore more