Browse FAQs

CLI CBUS power supply for 5000ETP10W

Published date: 18 December 2018

The unit doesn't come with a power supply

Required power connector is (12 V DC ± 5%, 1.5 A, right-angle connector type A 2.5 mm ID, center positive (+) ) or Ethernet port (For PoE: 802.3af)

We do not sell these power supplies

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.