undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
After I have configured a device on Wiser by SE, can I control this device on other phones at the same time?
When using devices in Zigbee connected to a Hub you can control your devices with any phone that supports the Wiser by SE App at the same time. The user must be logged in to an account that is a member of the home the devices are linked to.

When the devices are in BLE/Bluetooth the devices can only be controlled by one phone at a time. This is due to Bluetooth being a point to point connection and will require whoever is connected to the device to be disconnected before someone else can control it.

Note: You can’t be logged in to the App on more than one phone at a time on a single account.

Schneider Electric New Zealand

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: