undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
If network Internet access is disconnected, will an Automation created in the Wiser by SE App still execute?
This will depend on what is set under ‘condition met’. If the ‘condition met’ is set under ‘When weather changes’ this requires the Hub to have an internet connection to access these details. Without these details the Automation in this case will not execute.

If the ‘action’ is set to a notification, which also requires the Hub to have an internet connection, the Automation will work if it has other actions but will not send the notification.

Automations will be tagged as Local if not requiring internet access and if they do require internet access will have no label.

Zigbee devices communicate locally via the Wiser Hub and do not need internet access to function.
Wiser appwiser app

Schneider Electric New Zealand

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: