{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does the Wiser by SE App have a voice control function and if so, what functionality comes with Google, Siri or Alexa?
There is no built-in voice control function within the app. However, the following third-party voice controllers are supported for selected devices: Amazon Alexa, Google Assistant and Siri. To set up one of these services, open the slide-out menu, tap More Services and then tap one of the options under Voice Service. Follow the instructions in the app to set up your compatible voice controller. Note: Not all devices support voice control.

With Google voice controlyou can use commands to turn everything on or everything off, trigger moments, trigger separate devices, it can tell you what is switched on/off (switches are switches and dimmers are lights ie ‘hey google, what lights are on?’ ‘hey google, what switches are on’).

Siri is only compatible with Moments from Wiser by SE that have been linked to Siri.

Alexacan’t do everything on or off unless these are set as moments. When triggering moments they need to be turned ‘on’ ie Alexa turn ‘moment’ on as moments can only be triggered on and not off. You can also operate separate devices. Alexa can’t tell you what is turned on/off.

Schneider Electric New Zealand

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: