{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the Wiser Micro Module Dimmer have LED indication?
The Micro module Dimmer cannot be used with LED indication other than having the indicator always on. This is due to the Switch mechanism required for control being a momentary or Bell press type and using the 2nd terminal and a neutral connection would simply have the LED on permanently unless you were pressing the switch in.

Connecting the LED indicator to the ‘I’ terminal can create a pathway that interferes with the electrical signal the module is triggered with sometimes causing the switch control to not function or the module to behave erratically.

Connecting the LED indicator to the ‘L’ terminal means the module is then actively trying to dim the indicator also and with the led indicators being non-dimmable will cause an error in the module.

Schneider Electric New Zealand

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: