{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to enable a C-Bus Network Burden via Learn Mode?

This FAQ explains how to enable the software Network Burden via Learn Mode.

We can enable the software burden via the Toolkit software or by using a hardware burden, but if Toolkit isn’t scanning correctly and you don’t have a hardware burden, use the following process:

To enable the Software Network Burden via Learn Mode:
1. Find any Learn Mode output unit.
2. Press and hold down any of the Quick Toggle buttons, on any of the output
unit for 10 Seconds. The Unit and C-Bus LED begin to flash alternately.
3. Quickly double press any of the Quick Toggle buttons on any output units.
If successful, the Unit LED will flash rapidly and all the Quick Toggle
Buttons will turn on.
4. Double press the same Quick Toggle button again, and you will see that
the C-Bus LED change state. This particular unit is now in Super Learn
Mode. If the C-Bus LED is on the Software Burden is enabled.
5. Each time the same Quick Toggle button is double pressed the C-Bus LED
will toggle between on and off. This corresponds to the internal Network
Burden being turned on and off.
6. WARNING: When you exit learn mode, all of the Quick toggle buttons that
are on, will have the corresponding Group Addresses deleted. If you wish
to retain any previous programming on that particular unit, turn off each
Quick Toggle button before performing the next step with a single press.
7. To exit Super Learn Mode press and hold down any of the Quick Toggle
buttons for 2 seconds.

Note: The Unit Address of the unit that you put into Super Learn Mode will now have
the Unit Address 001 (01h).

The software Network Burden will now be successfully enabled on the output unit
that was put into Super Learn Mode.

Video Process:

Schneider Electric New Zealand

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: