FAQs

Ask a Question

Filter results

Clear
What can cause the motor to rock back and forth on a belt driven load?
Issue: What can cause the motor to rock back and forth on a belt drive, constant torque load? Product Line: All Altivar drives and Altistart soft...
What are the Share-UPS and Interface Expander modes of operation?
Issue What are the Share-UPS and Interface Expander modes of operation? Product Line   UPS Device Management AP9607/AP9607CB Interface Expander SmartSlot...
What is meant by Load profile in Compact NSX.
The load profile is stored in a counter. The counter counts up the number of of operating hours per load section. Example: One counter indicates the...
ATV12 will not run an unloaded or lightly loaded motor.
Issue: ATV12 drive is being used to test a small motor with no load on it.  Motor will reach 26 Hz and then starts shaking and making noise.  Drive...
Change default WebX ports in ClearSCADA
This article explains how the default WebX ports can be changed for the redesigned WebX interface in ClearSCADA 2015 R1 and later versions. The default...
What is the contact information for the Schneider Electric Leesport DBS products?
Issue: What is the number to get in contact with customer service and tech support for DBS units? Product Line: All DBS Environment: All models Cause:...
How is automatic restart enabled on an ATV61/ ATV71?
Issue: How is automatic restart enabled on an ATV61/ ATV71? Product Line: ATV61 ATV71 Environment: All Cause: System requirement. Resolution:  From...
Video: ATV212 - What does Fr-F or Fr-r indicate in the monitoring menu?
Issue: Video: ATV212 - What does Fr-F or Fr-r indicate in the monitoring menu? Product Line: ATV212 Altivar 212 Environment: All part numbers Cause:...
How is an Altivar VFD set to always run a particular speed when no reference input is connected?
Issue: How is an Altivar VFD set to always run a particular speed when no reference input is connected? Product Line: Altivar 12, 32, 312, 61, 71,...
Does the Energy Reading remain stored for ME range Energy Meters during power failure.
Yes, the Energy Readings remain stored for the ME range meters during power failure as they are stored in the EEPROM. EEPROM is nonvolatile memory...
Results 1 - 10 of 100