Schneider Electric makes it easier to achieve optimal efficiency with Easy Line
● SE introduces to the Philippine market its latest Easy Line Industrial Automation Offer
● Innovations available to the local market include Ease of Use, Basic Functionalities, Robustness, and Availability
Manila (Philippines), May 5, 2017 -- Schneider Electric, the global specialist in energy management and automation, launched the Easy Line Industrial Automation Offer in the Philippine market at the Ascott Hotel in Bonifacio Global City, Taguig City. The Easy Line is a range of automation and control products that have been developed to provide the following innovations to consumers in the emerging market segments: easiness of installation and selection; basic functionalities that focus on core performance, reduction of noncritical functions and locally required features; robustness that can stand harsh industrial environments; and, availability in an extensive network of distributors. Through the Easy Line, Schneider Electric ensures its consumers of innovation at every level.
In a report released by the UK government in October 2013, new economies will be playing a major role in the global economy particularly in the manufacturing industry, and with its newest Easy Line, Schneider Electric is making it possible for emerging economies to facilitate and maximize their growth efficiency.
Easy Line comes in three offerings: Automation Offer, Panel Builder Offer, and Universal Offer. The essential automation and control product lines include Human Machine Interface (HMI) and Power Supply, PLC, Drives, Push Buttons, and Control and Signaling. These products have not only been designed to operate in harsh environments but are also intuitive to set up and use. When just enough is just right.
Larry Cunanan, Head for Industry Business, Schneider Electric Philippines said: “By launching Easy Line, we at Schneider Electric are reinforcing our commitment to providing our customers with the right balance between their investment and our products’ performance. With these product offerings, we are our customers granting Innovation at Every Level and access to the best without sacrificing quality, robustness, availability, and service.”
With these product innovations, Schneider Electric remains optimistic in creating a positive impact on Filipino consumers as it reinforces its Life Is On campaign by providing markets with safety, reliability, efficiency, and sustainability
Below are the specific product offerings that Schneider Electric is making available to the Philippine market :
Universal Offer: Drive: Altivar Easy 310
● V asynchronous motors rated from 0.37 kW/0.5 HP to 11 kW/15 HP
● Easy use: short menu label and full parameter list; power off configurable, even in its packaging; using the Multi-Loader console; quick start guide for immediate setup
● Robustness: air flow system and resistance to disturbed power supplies; all cards are coated; working temp up to 55°C without de-rating; 10-year service life components
● Price effective
Universal Offer: Relay: Zelio Easy RXLM*LB
● Simple switching application
● Plug and Switch
● High level of robustness
● Cost effectiveness for your application
● Power & relays status indicator
Universal Offer: ABL2 Power Supply
● Output 24V DC (+/-10% adjustable)
● 7 power ranges from 35W to 350W
● Input voltage switch between 115VAC and 230VAC can be carried out automatically by 35/50/100W products. For the other products, switch button on the side face need to be adjusted to achieve this function.
● Green LED output indication
Panel Builder Offer: Push Button: Harmony Easy XA2
● Round, Metallic Looking Bezel, Pushbuttons and Switches,Ø22; Round, monolithic plastic Pilot Lights, Ø22
● Compactness with enough functions :PB, IPB, SS, KS, ES, PL
● Easy to install, connect and simple to choose
● Committed quality and robustness: CCC, IP54, millions of mechanical durability
● Price effective
Panel Builder Offer: Drive: Altivar Easy 610
● Special designed for pumps and fans speed control, from 0.75 to 160 kW, with below advantages:
● Easy use: 7 pre-programmed function blocks; easy integration on an enclosure door with remote display terminal ; colored control circuit terminals to avoid misuse
● Robustness: innovative cooling air flow separate from the printed circuit board to avoid dust and oil corrosion; electronic cards with protective coating; working temp: - 10…+ 60°C; IP40
● Price effective
Automation Offer: PLC: Modicon Easy M200 / M100
● M200: flexible and scalable small controller, up to 188 I/O, 2 axis motion control
● M100: basic and small logic controller , up to 40 I/O
● Removable terminal blocks, flexible I/Os, 2 cartridges, and up to 4 expansions for M200; relay and transistor outputs, Ethernet and serial line ports
● Easy use: standard USB port, USB powerless download; micro SD memory card (fast duplication); Run/stop switch
● Robustness: protected inputs, outputs and DC power supply; coated electronic; IP20
Automation Offer: Tower Light: Harmony Easy XVG column
● Essential touch screen panel, 2 sizes: 7“ & 10“
● Universal Ø 60 monolithic tower lights, 2 to 4 stages
● High practicality of features: 80dB buzzer , steady light with integral LED, 24V AC/DC
● Ergonomic design
● Extreme versatility of mounting
● IP42, CE certification
Automation Offer: HMI: Magelis Easy HMIGXU
● Essential touch screen panel, 2 sizes: 7“ & 10“
● Focus on core functions: TFT color screens; USB connection; Ethernet port
● Compact design (thickness 38mm max.)
● Easy installation and connection: anti-drop hooks; embedded USB locker; screw installation fasteners
● Robustness: PCBA coating for good behavior in polluted environments
About Schneider Electric
Schneider Electric is the global specialist in energy management and automation. With revenues of ~€25 billion in FY2016, our 144,000 employees serve customers in over 100 countries, helping them to manage their energy and process in ways that are safe, reliable, efficient and sustainable. From the simplest of switches to complex operational systems, our technology, software and services improve the way our customers manage and automate their operations. Our connected technologies reshape industries, transform cities and enrich lives. At Schneider Electric, we call this Life Is On.
● Innovations available to the local market include Ease of Use, Basic Functionalities, Robustness, and Availability
Manila (Philippines), May 5, 2017 -- Schneider Electric, the global specialist in energy management and automation, launched the Easy Line Industrial Automation Offer in the Philippine market at the Ascott Hotel in Bonifacio Global City, Taguig City. The Easy Line is a range of automation and control products that have been developed to provide the following innovations to consumers in the emerging market segments: easiness of installation and selection; basic functionalities that focus on core performance, reduction of noncritical functions and locally required features; robustness that can stand harsh industrial environments; and, availability in an extensive network of distributors. Through the Easy Line, Schneider Electric ensures its consumers of innovation at every level.
In a report released by the UK government in October 2013, new economies will be playing a major role in the global economy particularly in the manufacturing industry, and with its newest Easy Line, Schneider Electric is making it possible for emerging economies to facilitate and maximize their growth efficiency.
Easy Line comes in three offerings: Automation Offer, Panel Builder Offer, and Universal Offer. The essential automation and control product lines include Human Machine Interface (HMI) and Power Supply, PLC, Drives, Push Buttons, and Control and Signaling. These products have not only been designed to operate in harsh environments but are also intuitive to set up and use. When just enough is just right.
Larry Cunanan, Head for Industry Business, Schneider Electric Philippines said: “By launching Easy Line, we at Schneider Electric are reinforcing our commitment to providing our customers with the right balance between their investment and our products’ performance. With these product offerings, we are our customers granting Innovation at Every Level and access to the best without sacrificing quality, robustness, availability, and service.”
With these product innovations, Schneider Electric remains optimistic in creating a positive impact on Filipino consumers as it reinforces its Life Is On campaign by providing markets with safety, reliability, efficiency, and sustainability
Below are the specific product offerings that Schneider Electric is making available to the Philippine market :
Universal Offer: Drive: Altivar Easy 310
● V asynchronous motors rated from 0.37 kW/0.5 HP to 11 kW/15 HP
● Easy use: short menu label and full parameter list; power off configurable, even in its packaging; using the Multi-Loader console; quick start guide for immediate setup
● Robustness: air flow system and resistance to disturbed power supplies; all cards are coated; working temp up to 55°C without de-rating; 10-year service life components
● Price effective
Universal Offer: Relay: Zelio Easy RXLM*LB
● Simple switching application
● Plug and Switch
● High level of robustness
● Cost effectiveness for your application
● Power & relays status indicator
Universal Offer: ABL2 Power Supply
● Output 24V DC (+/-10% adjustable)
● 7 power ranges from 35W to 350W
● Input voltage switch between 115VAC and 230VAC can be carried out automatically by 35/50/100W products. For the other products, switch button on the side face need to be adjusted to achieve this function.
● Green LED output indication
Panel Builder Offer: Push Button: Harmony Easy XA2
● Round, Metallic Looking Bezel, Pushbuttons and Switches,Ø22; Round, monolithic plastic Pilot Lights, Ø22
● Compactness with enough functions :PB, IPB, SS, KS, ES, PL
● Easy to install, connect and simple to choose
● Committed quality and robustness: CCC, IP54, millions of mechanical durability
● Price effective
Panel Builder Offer: Drive: Altivar Easy 610
● Special designed for pumps and fans speed control, from 0.75 to 160 kW, with below advantages:
● Easy use: 7 pre-programmed function blocks; easy integration on an enclosure door with remote display terminal ; colored control circuit terminals to avoid misuse
● Robustness: innovative cooling air flow separate from the printed circuit board to avoid dust and oil corrosion; electronic cards with protective coating; working temp: - 10…+ 60°C; IP40
● Price effective
Automation Offer: PLC: Modicon Easy M200 / M100
● M200: flexible and scalable small controller, up to 188 I/O, 2 axis motion control
● M100: basic and small logic controller , up to 40 I/O
● Removable terminal blocks, flexible I/Os, 2 cartridges, and up to 4 expansions for M200; relay and transistor outputs, Ethernet and serial line ports
● Easy use: standard USB port, USB powerless download; micro SD memory card (fast duplication); Run/stop switch
● Robustness: protected inputs, outputs and DC power supply; coated electronic; IP20
Automation Offer: Tower Light: Harmony Easy XVG column
● Essential touch screen panel, 2 sizes: 7“ & 10“
● Universal Ø 60 monolithic tower lights, 2 to 4 stages
● High practicality of features: 80dB buzzer , steady light with integral LED, 24V AC/DC
● Ergonomic design
● Extreme versatility of mounting
● IP42, CE certification
Automation Offer: HMI: Magelis Easy HMIGXU
● Essential touch screen panel, 2 sizes: 7“ & 10“
● Focus on core functions: TFT color screens; USB connection; Ethernet port
● Compact design (thickness 38mm max.)
● Easy installation and connection: anti-drop hooks; embedded USB locker; screw installation fasteners
● Robustness: PCBA coating for good behavior in polluted environments
About Schneider Electric
Schneider Electric is the global specialist in energy management and automation. With revenues of ~€25 billion in FY2016, our 144,000 employees serve customers in over 100 countries, helping them to manage their energy and process in ways that are safe, reliable, efficient and sustainable. From the simplest of switches to complex operational systems, our technology, software and services improve the way our customers manage and automate their operations. Our connected technologies reshape industries, transform cities and enrich lives. At Schneider Electric, we call this Life Is On.