How can we help you today?

Changing the color on the network display setup returns an 'illegal function call' error.

Issue
Changing the color on the network display setup returns an 'illegal function call' error.

Product Line
'ProWORX NxT version 2.2'

Environment
Windows 7

Resolution
If you try to change the color on the network display setup, 'ProWORX NT' could return an 'illegal
function call' error.

This can happen if the Windows display is configured for a setting that is higher than what the software
was originally designed to be used with. 'ProWORX NxT' is based upon Windows NT architecture and
it is designed for a 16 bit screen resolution of 1024 x 768.

To resolve the issue, change the resolution from 32 bit to 16 bit display. If the problem still occurs,
try changing the compatibility mode to 256 colors. by using the following steps:

  • Right click on the 'ProWORX NxT' shortcut.
  • Click on 'Properties'.
  • Click on the tab named 'Compatibility'.
  • Select option for 'Run In 256 colors' under 'display Settings.
  • Click OK to close the 'Properties' window..

Schneider Electric Philippines

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center