Como o podemos ajudar hoje?

Video: Why am I unable to edit my Vista diagram?

Issue
A user would like to modify an existing Vista diagram but is unable to edit any diagram objects.

Product Line
ION Enterprise 6.0
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Vista

Cause
The 'Show Toolbox' option must be selected within the Options drop down menu.  The user must be logged in with a Supervisor level account in order to access this setting.

Resolution
Click the Options drop down menu and select the 'Show Toolbox' option.